Project 1 - Circuit A

Blinking an LED

Project 1: Light Circuit 1A: Blink an LED Circuit 1B: Potentiometer Circuit 1C: Photoresistor Circuit 1D: RGB Night-Light Project 2: Sound Circuit 2A: Buzzer Circuit 2B: Digital Trumpet Circuit 2C: Simon Says Game Project 3: Motion Circuit 3A: Servo Motors Circuit 3B: Distance Sensor Circuit 3C: Motion Alarm Project 4: Display Circuit 4A: OLED "Hello, World!" Circuit 4B: Temperature Sensor Circuit 4C: DIY Who Am I? Game Project 5: Robot Circuit 5A: Motor Basics Circuit 5B: RC Robot Circuit 5C: Autonomous Robot

Project Overview

You can find LEDs in just about any source of light, from the bulbs lighting your home to the tiny status lights flashing on your home electronics. Blinking an LED is the classic starting point for learning how to program embedded electronics. It’s the “Hello, World!” of microcontrollers. In this circuit, you’ll write code that makes an LED blink on and off.

Project 1 - Circuit A

1 LED, 1 330 ohm Resistors 2 jumper wires


New Components

Light-Emitting Diodes (LEDs)

LEDs are small lights made from a silicon diode. They come in different colors, brightnesses and sizes. LEDs (pronounced el-ee-dees) have a positive (+) leg and a negative (-) leg, and they will only let electricity flow through them in one direction. LEDs can also burn out if too much electricity flows through them, so you should always use a resistor to limit the current when you wire an LED into a circuit.

LEDs

Resistors

Resistors resist the flow of electricity. You can use them to protect sensitive components like LEDs. The strength of a resistor (measured in ohms) is marked on the body of the resistor using small colored bands. Each color stands for a number, which you can look up using a resistor chart. One can be found in our guide on resistor markings.

New Concepts

Polarity

Many electronics components have polarity, meaning electricity can (and should) flow through them in only one direction. Polarized components, like an LED, have a positive and a negative leg and only work when electricity flows through them in one direction. Some components, like resistors, do not have polarity; electricity can flow through them in either direction.

Polarity of an LED

OHM’s Law

OHM’S LAW describes the relationship between the three fundamental elements of electricity: voltage, resistance and current. This relationship can be represented by this equation:

V = I • R

V = Voltage in volts

I = Current in amps

R = Resistance in ohms (Ω)

This equation is used to calculate what resistor values are suitable to sufficiently limit the current flowing to the LED so that it does not get too hot and burn out.

Digital Output

Digital Output pins on a RedBoard

When working with microcontrollers such as the RedBoard, there are a variety of pins to which you can connect electronic components. Knowing which pins perform which functions is important when building your circuit. In this circuit, we will be using what is known as a digital output. There are 14 of these pins found on the RedBoard. A digital output only has two states: ON or OFF. These two states can also be thought of as HIGH or LOW, TRUE or FALSE. When an LED is connected to one of these pins, the pin can only perform two jobs: turning on the LED and turning off the LED. We’ll explore the other pins and their functions in later circuits.

New Ideas

ELECTRICAL SAFETY: Never work on your circuits while the board is connected to a power source. The SparkFun RedBoard operates at 5 volts, which, while not enough to injure you, is enough to damage the components in your circuit.

COMPONENT ORIENTATION & POLARITY: Instructions on how to orient each of the new components will be given before each circuit diagram. Many components have polarity and have only one correct orientation, while others are nonpolarized.

Polarized component graphic

Hookup Guide

READY TO START HOOKING EVERYTHING UP? Check out the circuit diagram and hookup table below to see how everything is connected.

Circuit diagram for LED

Hookup Tables

Many electronics beginners find it helpful to have a coordinate system when building their circuits. For each circuit, you’ll find a hookup table that lists the coordinates of each component or wire and where it connects to the RedBoard, the breadboard, or both. The breadboard has a letter/number coordinate system, just like the game Battleship.

Hookup table examples

D34 to J2…means one end of a component connects to digital pin 34 on your RedBoard and the other connects to J2 on the breadboard.

Programming the RedBoard

The SparkFun RedBoard IoT is programmed using MicroPython and this project uses MicroPython commands to blink the LED in the circuit we just created. Before this is possible, a MicroPython tool is needed to communicate with the RedBoard.

Selecting a MicroPython Tool

Our suggested tool is the Thonny IDE. For instructions on how to install and use Thonny, check out our Thonny Guide.

The first step to enter commands on the RedBoard is to select a tool that allows direct interaction with MicroPython.

While a variety of methods exist to communicate with the RedBoard, the following tools are the most popular: Thonny, PyCharm and the command mpremote.

Once you select and install a tool, make sure your RedBoard is connected to your computer, and the micropython tool is connected to the RedBoard. Once connected, you should have access to the MicroPython REPL command line.

Remember that the source files for each SIK circuit are already on your IoT RedBoard RP2350 in the “sik_examples” folder. So if using the suggested Thonny tool, you can select the example for this circuit and run it directly with the green “run current script” button rather than executing lines individually.

Entering MicroPython Commands

Step 1 - Setup

To blink the LED, we need to enable the board pin 34 (the pin that the LED is connected to in the circuit).

To do this we load the Pin definition for the board

from machine import Pin

Now create a Pin variable for the LED pin, number 13. Also define it as an output pin, so we can turn it on and off

led_pin = Pin(34, Pin.OUT)

We turn the LED on by setting the pin value to high or on

led_pin.high()

And to turn the LED off, we set the pin to low

led_pin.low()

To blink the LED, we can turn it on, wait a period of time and then turn it off. This is done by sleeping between the on and off commands.

To do this in MicroPython, we need a sleep function. Let’s load the sleep function, which will sleep for a number of seconds.

from time import sleep

Now lets blink the LED - sleeping for 1 second between turning the LED on and off

led_pin.high()
sleep(1)
led_pin.low()
sleep(1)
led_pin.high()
sleep(1)
led_pin.low()

Now we have blinked the LED!

Now we’ll present the idea of a for loop. A loop repeats a statement for a number of specified times.

To blink our LED 10 times, use the following command:

for i in range(10):
    led_pin.high()
    sleep(1)
    led_pin.low()
    sleep(1)

When this command runs, it blinks the LED 10 times by setting the LED high, then low and sleeping in between each step.

You’ve Completed Circuit 1A!

Continue to circuit 1B to learn about analog signals and potentiometers

Next up, reading a potentiometer

Video Walkthrough